Digital Microscopes
Tilted Observation and 3D Measurement of Microneedles and Their Molds
Microneedles are not just used in the field of medicine, but also in the field of cosmetics to easily and painlessly administer liquid medicine to the epidermis. Large strides are being made in needle technology, allowing new types of needles to be developed for specific uses, such as needles that dissolve inside the human body. Because of the increase in technological advancements, there is also an increase in demand, making high quality and reliability necessary for mass production. This section introduces basic microneedle knowledge, including types of needles and their uses, as well as examples of observing and inspecting molds used in production.
What Is a Microneedle?
Microneedles are microscopic needles with diameters and lengths both less than 1 mm (0.04"). Generally, a large number of microneedles are arranged tightly in a grid. In dermal administration, the microscopic needles pierce the skin, passing through the stratum corneum on the skin surface, allowing for direct administration to the epidermis, which differs from general ointments and medicinal patches.
Microneedle applications
Microneedles are used not just for medication such as anesthetization, insulin, vaccines, and hyaluronic acid; but also widely in the administration of solutions for non-medicinal cosmetic purposes.
Microneedle advantages
Administration to multiple points at a shallow depth on the skin (the epidermis) is possible, differing from the use of a general hypodermic needle, which administers the medicine to a single point in the dermis or lower in the hypodermis. A corresponding advantage is that the solution can be administered easily and painlessly because the needles do not reach the dermis, which has many pain receptors.
Get detailed information on our products by downloading our catalog.
View Catalog
Microneedle Types and Applications
Conventionally, the popular material for needles has been metal, but the use of microneedles produced through various methods; having various shapes; and made of various materials such as biomass plastic, biodegradable plastic, and water-soluble polymers is becoming commonplace. Typical microneedle classifications are as follows.
- Non-dissolving (biodegradable) microneedles
These microneedles are made of polyglycolic acid (PGA) and polylactic acid (PLA), polymers used in medical devices, and the solution is applied to the tips of the needles. This type is expensive but is used as the optimal microneedle for solutions and vaccines that must be administered in extremely small amounts. Typical applications include the administration of influenza vaccines and therapeutic drugs for hepatitis C, diabetes, and osteoporosis. - Dissolving microneedles
These microneedles use microscopic needles made from water-soluble polymers (such as hyaluronic acid), peptides, and protein drugs. In most cases, a sheet of microneedles is affixed to the skin, whose moisture then dissolves the needles, administering the solution to the epidermis. One typical application is the administration of local anesthetics, but the use of these microneedles for cosmetic purposes such as administering hair growth agents and improving blemishes and wrinkles has become more and more common in recent years.
We’re here to provide you with more details.
Reach out today!
Examples of Tilted Observation and 3D Measurement of Microneedles and Their Molds
Microneedle production methods vary depending on their type and material. Because these needles require high accuracy, when forming them with molds it is important to check the molds for wear and flaws in order to prevent defects and to identify the causes of defects that do occur.
In addition to molds, microneedle production methods also include creating needles on sheets with a dispenser, laser processing, and 3D printing. There are diverse methods, and new technologies are being researched actively. Regardless of how microneedles are produced, the observation, measurement, and evaluation of the 3D shapes of the needles are vital in the quality management, quality assurance, and research and development of microneedles.
However, it was very difficult to observe and measure the 3D shape of precisely arranged microscopic needles and molds with conventional microscopes and measuring instruments.
KEYENCE has continued developing new digital microscopes for more than 30 years, putting to use the testimonials of on-site operators in order to solve their problems. The ultra-high accuracy VHX Series 4K digital microscope is a next-generation microscope resulting from our latest technologies and the know-how we have accumulated over all these years.
Tilted observation of a microneedle mold
Molding is one typical microneedle production method. Mold management is vital in ensuring that each and every one of the many arranged microscopic needles is produced free of problems and defects.
However, molds have precise and complicated three-dimensional shapes, so with conventional microscopes it was necessary to use a jig to secure and tilt these small targets on the stage. It was also necessary to take a lot of time and effort to determine the lighting conditions due to the diffuse reflections of light characteristic to the metal material.
The VHX Series 4K digital microscope uses a free-angle observation system with XYZ motorized stage to enable tilted observation with easy field-of-view alignment, rotation, and oblique axis motion. The target stays centered in the field of view even if the lens is tilted or rotated. The result is tilted observation that is both easy and smooth.
The VHX Series is equipped with an optical system and a 4K CMOS image sensor that combine high resolution with a depth of field that is at least 20 times larger than general optical microscopes. The large depth of field allows entire three-dimensional targets to be brought into focus. In addition, the depth composition function can be used to easily capture images that are fully focused throughout the entire field of view, even when observing three-dimensional targets at high magnifications. Of course, this depth composition function can also be used during tilted observation.
Furthermore, this product is equipped with the Multi-lighting function, which automatically acquires the data of multiple images captured with omnidirectional lighting at the press of a button. Observation can be started immediately just by selecting the image that matches the purpose, which dramatically reduces the condition determination time required until now.
The high performance and diverse functions described above allow for easy and fast tilted observation with high-accuracy 4K images, even when observing the 3D shapes of microneedle molds.
Ring illumination (100x)
Tilted observation of microneedle molds with the VHX Series 4K digital microscope
3D measurement of microneedles
The VHX Series allows not just for high-resolution observation, but also fast 3D shape measurement.
This product instantaneously composes the image from multiple images with varying focus positions, allowing it to display 3D images that even capture textures and surface roughness. The result is that the 3D image displayed on the screen can be rotated to any angle for observation without having to move the target on the stage or change the angle of the lens.
Furthermore, 3D measurements can be performed from the high-accuracy 3D information that has been acquired, and profile measurements can be performed simply by selecting a cross section with the mouse. Sub-micrometer level measured values can be acquired for 3D measurements, cross-section shapes, and surface irregularities of the delicate microscopic needles in a non-destructive, non-contact manner.
Coaxial illumination (500x) + 3D display and profile measurement
3D display and profile measurement on the VHX Series 4K digital microscope
We’re here to provide you with more details.
Reach out today!
A 4K Digital Microscope That Strongly Supports the Quality Control and Research and Development of Microneedles
The VHX Series 4K digital microscope allows for 4K observation, imaging, and 3D shape inspection of microneedles.
With its high performance, functionality, and usability, the VHX Series can dramatically optimize microneedle production work, which requires high reliability and safety and is extremely competitive in the field of research and development.
For additional info or inquiries about the VHX Series, click the buttons below.
Get detailed information on our products by downloading our catalog.
View Catalog