CMM (Coordinate Measuring Machine)
- In-Process Inspection
- Final Inspection
- Machine Alignment
- Reverse Engineering
- On Machine Measurement for Efficient In-Process Inspection
- Die Casting Inspection: Ensuring Dimensional Accuracy
- CMM for Heavy Machinery
- Vernier Calipers/Height Gauges
- Enhance Receiving Inspection
- How to Select the Right: Cost & Accuracy
Laser Tracker
Introducing KEYENCE’s WM Series, a wide-area CMM that resembles the look and functionality of a laser tracker without the common issues. This device has a dedicated wireless probe that eliminates movement restrictions when measuring large targets. Measurements by the laser tracker can also be performed virtually anywhere with no need to take targets to a metrology lab, helping to reduce the time spent on measurement and improving operating rates. In addition, the laser tracker has great accuracy—in the μm range—eliminating variations in measurement results for parts with complex shapes requiring high accuracy, including turbine blades.
What is a Laser Tracker?
A laser tracker is a measuring device that works by projecting a laser beam onto an optical target in contact with an object being measured. The device then determines the three-dimensional position of the target. The optical targets are known as “retroreflective” because they reflect the laser tracker beam back to its emitted origin point – typically known as a spherically mounted retroreflector (SMR). Dimension values, angles, geometrical tolerances, etc., are determined by software that calculates the 3D coordinates of the retroreflector.
Understanding a Laser Tracker
Laser trackers are characterized by the ability to measure large objects. Laser trackers generally have a measuring range of more than 10 m 30', whereas a standard arm-type CMM has a maximum measuring range of a couple of meters. It is useful in situations where you want to measure large objects such as airplanes, parts of large equipment, and parts produced by double-column, 5-face milling machines.
Laser Tracker Components
The laser tracker measurement components are generally divided into four parts.
A PC to run laser tracker operation software, a camera body that integrates a light-emitting unit and a light-receiving unit, a tripod that supports it, and a retroreflector (SMR) that contacts the object to be measured.
We’re here to provide you with more details.
Reach out today!
How Does a Laser Tracker Work?
Modern laser trackers use optical technology to follow targets and calculate precise coordinates through advanced algorithms. These devices maintain constant contact with the retroreflector during measurement sequences.
The laser tracking system relies on interferometry to ensure consistent accuracy. When the retroreflector moves, the system automatically adjusts to maintain signal strength. This allows operators to measure curved surfaces without losing contact with the target.
Temperature conditions can impact the accuracy of laser measurements, so modern systems incorporate environmental compensation features. These adjustments maintain reliability across different working conditions.
The laser tracker determines the center coordinates of the retroreflector (SMR) by using distance and angle data gathered from the horizontal and vertical two-axis rotary encoders. The laser tracker body follows the laser by rotating along both the horizontal and vertical axes.
The retroreflector (SMR) has a mirror surface inside, and no matter what angle the laser light is received, it returns the light in the direction from which it came. The retroreflector (SMR) is a true sphere designed so that light always reflects from its center, allowing the laser tracker to precisely determine the sphere’s center coordinates.
The KEYENCE WM Series functions similarly to a laser tracker, using line-of-sight tactics to take measurement points, but rather than using a laser beam, the WM Series utilizes near-infrared light to see the probe and take points. This reinvents classic techniques for measuring large parts and eliminates the common issues, such as warm-up time and ease of use.
Discover more about this product.
Click here to book your demo.
Laser Trackers vs Portable Arms
The choice between laser trackers and measuring arms depends on application and operational needs. Traditional measuring arms present operational challenges for some laser tracker applications. These systems have limited measurement range and routing capabilities. Tool mobility becomes constrained by the arm's mechanical structure.
Portable and handheld measurement units like the WM-6000 Series offer enhanced flexibility. With a wide measurement range and no routing limitations, these wireless units are easy to set up and ready to use with no specialized training required.
Accuracy and Range Comparison
When comparing tracker vs arm performance, laser measurement accuracy varies by distance and positioning. Traditional arms perform best in controlled environments where mechanical stability ensures consistent results. In contrast, portable units provide greater versatility while still delivering the measurement accuracy required for quality control applications.
Portability, Speed, and Cost Considerations
Despite their name, portable laser tracker systems like the WM-6000 Series eliminate setup time and provide instant measurement capabilities. Traditional arms require fixed positioning and calibration procedures. The wireless design reduces operational costs by eliminating specialized training requirements.
Advantages of KEYENCE Laser tracking CMM and 3D scanner
- Ease of Operation: Unlike conventional laser trackers, the KEYENCE WM Series has user-friendly software that can be used by anyone with minimal training. Its ability to save programs for repeat parts and continuously measure without interruptions streamlines the inspection process.
- Speed and Efficiency: Traditional laser tracker machine setups require extensive preparation. With the WM Series, setup time is just a matter of a few minutes.
- Cost-Effective Solution: The WM Series reduces total ownership costs through simplified operation and maintenance. The portable laser tracker design eliminates the need for dedicated measurement rooms, allowing for quality control integration into production workflows.
Single-Person Measurement of Large Targets
The WM Series uses a handheld probe, making it possible for individual workers to measure large parts and equipment that would require several people with conventional laser trackers. In addition to a wide measurement range, the freedom of movement provided by the wireless probe allows for fast measurement, even with time-consuming and difficult measurements, helping to reduce both effort and costs.
Fast, Highly Accurate Measurements
The WM Series can be used to measure 3D features and GD&T over a wide measurement range in less time and with higher accuracy than tape measures, calipers, or micrometers. The WM Series is also able to import 3D CAD data for comparing differences with actual targets.
On-the-Spot Measurements With No Need for a Metrology Lab
Because the WM Series is portable and can be installed virtually anywhere, it eliminates the need to move targets to a metrology lab/quality room and opens the door to a wide variety of applications, such as checking targets on manufacturing machines and performing periodic inspections during operation.
User-Friendly
The WM Series was created with users in mind, from beginners to metrology experts. First off, KEYENCE’s WM Series only requires three simple steps: select the tool on the touch screen, touch the probe to the part, and press measure. If that’s not intuitive enough, there are video and picture tutorials that walk through the processes and different functions. A major advantage for ease of operation and understanding is the augmented reality measurement guidance, which overlays the measurement data over a picture of the physical part.
Get detailed information on our products by downloading our catalog.
View Catalog
Key Features of KEYENCE’s Laser Tracking CMM System
Statistical Analysis
KEYENCE’s WM Series, similar to a laser tracking system, has built-in statistical analysis software. This feature reduces time spent on manual statistical analysis, separate from the measuring process. The measuring tool’s statistical analysis function can extract these analyses:
- Maximum/minimum value
- Pass/fail
- Average
- σ, 3σ, 6σ
- Cpk
- Increased variation trends
- Upward/downward measurement trends
- Periodic fluctuations
- Histograms
3D CAD Data Comparison
The WM Series features software that seamlessly compares measured parts to CAD. While traditional laser trackers capture individual points, the WM’s auto-trigger function rapidly collects dense point data. This enables the creation of highly detailed point clouds and color maps, making it easy to visualize profiles and contours and quickly verify part accuracy against CAD models.
Wide Range of Measurement
The WM Series has a wide measurement range that is suitable for large parts. The laser tracker measurement tool has a horizontal measurement range of 15 m and a vertical measurement range of 12.5 m. Also, since the device is portable, its setup can be easily adapted to meet the demands of large part inspection, such as on a tripod, cart, or granite table.
Temperature Compensation Function
The temperature compensation function of the WM Series can adjust its temperature to match that of a climate-controlled measuring room. With this feature, measuring can continue even if there isn’t readily available access to a separate measuring room.
We’re here to provide you with more details.
Reach out today!
Laser Tracker Case Studies
Application Example 1: Dimensional Measurement of H-shaped Steel Beams
H-shaped steel beams are an essential material in civil engineering and building construction. Conventional methods for measuring these beams involve multiple workers using calipers or tape measures, which can be time-consuming. KEYENCE’s laser tracker makes it possible to measure the shape, joined section finish, and welding shrinkage amount using the wireless probe.
Application Example 2: Leveling of Industrial Machinery
Leveling is an important step when installing industrial machinery, equipment frames, or base frames. Equipment or devices installed at an angle could lead to malfunctioning products or parts, or the equipment itself could become damaged due to unexpected loads. Using KEYENCE’s laser tracker makes it easy for even individual workers to perform leveling quickly, with significantly reduced time spent on setup.
Application Example 3: Vacuum Chamber Dimensional Measurement
Vacuum chamber quality depends greatly on semiconductor device performance. Leaks (vacuum leaks) that allow air to enter through gaps in the vacuum chamber and degassing caused by poor bonding or other causes must be prevented, as these factors could lead to defective semiconductor devices. Using a laser tracker to accurately measure the shapes and dimensions both before and after assembly can significantly improve quality.
Discover more about this product.
Click here to book your demo.
Laser Tracker Application Examples:
Example 1: Large Valve
With a large valve, the laser tracker can measure the distance between the center and the edge as well as the intersection point. Valves also have holes that can be measured by using the plane function.
Example 2: Heat Exchanger
On a heat exchanger, the plane function on the laser measuring tool can be used to measure the flatness.
Example 3: Machine Tool Component (Column)
With a machine tool component column, the plane function on the laser tracker is often utilized to measure the flatness or parallelism.
Example 4: Bridge Components
On a bridge component, the laser tracker can measure the top with the plane function. If there are slot centers, the laser tracker can use the rectangular slot center or the circle center function.
FAQs About Laser Tracker
How do laser trackers work?
A laser tracker emits a laser beam toward a retroreflective target, often a spherically mounted retroreflector (SMR), which is placed on the object that is being measured. The laser light is reflected by the SMR, and upon re-entry into the tracker, a distance meter within calculates the precise distance between the tracker and the retroreflector. The captured coordinate data is then transmitted to metrology software, which establishes the X, Y, and Z coordinates for the measured point to construct dimensional measurements like lines, diameters, angles, etc. The KEYENCE WM Series is a new take on a laser tracker, allowing large parts to be measured using only infrared light.
How accurate is laser tracker measurement?
Laser trackers have the potential to be incredibly accurate in the Y axis. While still accurate, because of the technology used by laser trackers, the accuracy for laser trackers is lesser in the X & Z axes. Conversely, KEYENCE CMMs are the opposite, being more accurate in the X and Z, and less accurate in the Y.
What is the range of a laser tracker?
Laser trackers can have a substantial range. Laser trackers are ideal for measuring the length of sizable parts. For example, they’re great for parts in the construction, aerospace, & naval industries. The KEYENCE WM Series is great for parts in the 6-82-foot range. For most companies, a laser tracker is "overkill" for that type of application. The WM Series can accommodate larger parts, up to ~ 82 feet wide, in a single setup. The WM Series was designed to fill a gap where parts are too large or cumbersome for traditional CMMs that need quick or complex inspection, and parts that are smaller than necessary for laser trackers. The WM maintains accurate measurements, ease of use, and no warm-up time, which is unparalleled to alternative products.
What types of probe tips can a CMM use?
KEYENCE CMMs use M5 threaded, spherical (or hemispherical) probe tips. Because of the technology used, the part of the tip touching the feature must be spherically rounded, but any probe tip of this fashion can work with KEYENCE's CMMs.
Where can a wide-area CMM be used?
KEYENCE's CMMs are portable, so they can be used anywhere. Ideally, they should be used in environments with 32-104 degrees Fahrenheit with 20-80% relative humidity. While our systems are almost exclusively used on the shop floor or in a quality lab, we have successfully used our systems outdoors, despite that not being their traditional use.
Do laser trackers require frequent calibration?
Most laser trackers require regular calibration to maintain laser measurement accuracy, typically every six to 12 months, depending on usage.
Can laser trackers measure in real-time during machining?
Traditional laser tracker machine setups cannot measure during active machining due to vibration. However, portable laser tracker systems can measure between cycles.
How does environmental vibration affect tracker performance?
Vibration significantly impacts the accuracy of laser measurements, requiring a stable mounting. The laser tracking system includes filtering for minor vibrations.
What types of objects are ideal for measurement with a laser tracker?
Large components in aerospace, automotive, and construction represent ideal applications for laser trackers.
How does the WM Series handle large object measurements?
The WM Series extends laser trackers' capabilities to medium-sized objects. Its portable laser tracker design allows flexible positioning around complex shapes.
We’re here to provide you with more details.
Reach out today!
Related Products
Scroll
Related Downloads
-
WM-6000 series Wide Area CMM Catalog
Brochure for the WM-6000 series Wide-Area CMM. A portable setup with a wireless handheld probe that enables users measure large parts and equipment.
Scroll
Related Information
Types
Applications
- In-Process Inspection
- Final Inspection
- Machine Alignment
- Reverse Engineering
- On Machine Measurement for Efficient In-Process Inspection
- Die Casting Inspection: Ensuring Dimensional Accuracy
- CMM for Heavy Machinery
- Vernier Calipers/Height Gauges
- Enhance Receiving Inspection
- How to Select the Right: Cost & Accuracy