Weldment Dimensional Inspection for Large Fabrications

Key Takeaways

  • Weldment dimensional inspection verifies that a welded part's size, hole positions, and geometry match the drawing after welding and fabrication.
  • Large weldments are hard to inspect because they exceed the size of fixed CMMs, and attached plates and gussets block tape measures and hand tools.
  • A large-part CMM such as the KEYENCE WM Series lets one operator measure parts up to 25 m (82 ft) in place, using a wireless handheld probe.
  • In published KEYENCE case studies, fabricators cut inspection time to 1/10 of previous methods and reduced inspection labor and time costs by 40%.

Weldment dimensional inspection is the process of measuring a welded part or structure to confirm that its dimensions, hole positions, and geometric tolerances match the drawing. For large welded frames and steel structures, the most practical approach is to measure the part where it sits, using a portable system that one person can operate.

This page explains what gets measured on a weldment, why large fabrications are difficult to inspect, and how a KEYENCE wide-area CMM handles the job on the shop floor.

What Is Weldment Dimensional Inspection?

Weldment dimensional inspection checks the size and shape of a finished or partially finished welded part. It answers one question: does the fabricated part match the drawing closely enough to assemble, machine, or ship?

A weldment is any part made by welding multiple pieces together, such as a machine frame, a structural steel member, or a construction-equipment boom. Because welding joins many separate pieces, small errors in cutting, fit-up, and welding can add up across the part.

Dimensional Inspection vs. Weld Quality Inspection

These are two different checks. Dimensional inspection measures the whole part's geometry, while weld quality inspection looks at the weld bead itself. For bead-level checks, see machine vision for weld inspections.

Weldment dimensional inspection Weld quality inspection
What it checks
Weldment dimensional inspection
Overall size, hole positions, angles, and GD&T of the full part
Weld quality inspection
The weld bead: its presence, position, and appearance
Typical question
Weldment dimensional inspection
"Is this frame built to the drawing?"
Weld quality inspection
"Is this weld acceptable?"
Typical tools
Weldment dimensional inspection
Tape measures, jigs, CMMs, wide-area CMMs, 3D Scanners
Weld quality inspection
Vision systems, profile measurement

What Features Are Checked on a Large Weldment?

Most weldment drawings call out a mix of distances, positions, and geometric tolerances. Common inspection points include:

  • Overall length, width, and height – the outer envelope of the part.
  • Diagonal distances – used to confirm an assembled frame is square.
  • Hole center positions – where bolts, pins, or mating parts will attach.
  • Scribed line extension points – layout marks that locate features on structural steel.
  • GD&T callouts – geometric dimensioning and tolerancing, a standard system for specifying flatness, position, perpendicularity, and other form requirements.
  • Surface shape – the form of curved or complex surfaces, compared against the intended design.

Why Is Measuring Large Weldments So Difficult?

Large weldments are difficult to measure because they are too big to bring to a measuring machine and too complex to measure accurately by hand. Several problems tend to stack up.

The Part Is Bigger Than the Machine

Weldments for construction machinery and steel structures can exceed 10 m in length. Parts this size do not fit on a conventional fixed CMM, and they are often beyond the reach of an arm-type CMM without repositioning.

Attached Plates Get in the Way

Gusset plates and attached pieces often sit between the two points being measured. A tape measure can't pass through them, which makes accurate readings difficult.

Manual Methods Take a Crew

Measuring a long steel member with a tape typically needs one person at each end, another for intermediate points, and someone to record values. Those people are pulled away from production every time a part needs checking.

Jigs and Results Are Hard to Trust

Many shops build a dedicated inspection jig for each product, which takes labor and storage space. Hand measurements also vary between operators, leaving doubt about whether the values are correct.

How Are Large Weldments Traditionally Inspected?

Most fabricators rely on hand tools, custom jigs, or arm-type CMMs. Each works in some situations but has clear limits on large parts.

Method How it works Limitations on large weldments
Tape measures and hand tools
How it works
Operators measure point-to-point by hand
Limitations on large weldments
Needs several people; blocked by plates; results vary by operator
Inspection jigs
How it works
A custom fixture confirms key features fit
Limitations on large weldments
Built per product; takes labor and storage space
Arm-type CMM
How it works
A jointed arm with a probe measures within its reach
Limitations on large weldments
Limited range; must be repositioned around large parts
Fixed CMM
How it works
The part is placed on a machine in a lab
Limitations on large weldments
Large weldments don't fit; moving the part adds time

For a broader comparison of measuring machine types, see portable vs. fixed CMMs.

How Does a Wide-Area CMM Measure Weldments?

A wide-area CMM uses a camera to track the position and orientation of a handheld probe in 3D space. The operator touches or scans the weldment, and the system records each point's coordinates without the part ever moving.

The KEYENCE WM-6000 Series offers a measurement range of up to 25 m (82 ft), with a measurement volume of 25 m wide × 12.5 m deep × 12.5 m high. Its wireless probes remove cable-routing limits, so the operator can walk around the full weldment. (Wireless communication between the camera and PC uses the WM-WL WLAN unit.)

Contact Probe vs. Laser-Scanning Probe

Probe Best for Weldment examples
Contact probe
Best for
3D and GD&T measurement of specific points
Weldment examples
Hole centers, diagonals, mounting positions, scribed lines
Laser-scanning probe
Best for
Full-part profile and shape measurement
Weldment examples
Curved surfaces, complex shapes, overall form

A Typical Weldment Inspection Workflow

  • 1.
    Set up the camera near the weldment. The part stays where it is on the shop floor.
  • 2.
    Establish the part's reference by probing datum features called out on the drawing.
  • 3.
    Measure points and features with the contact probe, controlling the operation from the handheld probe.
  • 4.
    Scan complex surfaces with the laser-scanning probe where shape matters.
  • 5.
    Move the camera if needed. The Camera Movement function makes measurement easy even for large targets.
  • 6.
    Review the report. The system automatically records measurement data and creates inspection reports.

Why One Operator Is Enough

Because the camera tracks the probe, there is no tape to hold at the far end. KEYENCE describes the WM Series as enabling single-person measurement for large parts, assemblies, and equipment. Learn more in reasons for selecting the wide-area CMM WM Series.

What Results Have Fabricators Seen?

Published KEYENCE case studies show large reductions in inspection time and labor for welded and fabricated parts.

Browse more examples on the WM Series applications page.

Where Does Dimensional Inspection Fit in Fabrication?

Dimensional checks are most useful at the points where an error is still cheap to fix. Common checkpoints in a weldment workflow include:

  • After fit-up, before final welding – confirm pieces are positioned correctly while they can still be adjusted.
  • After welding – confirm the finished weldment still matches the drawing.
  • Before machining – confirm there is enough material in the right places before the part goes to a machine tool.
  • Before shipping – document conformance for the customer. See CMM final inspection applications.

Saved scan data also supports traceability. It lets a team answer later questions about a part without measuring it again.

Frequently Asked Questions

Q What is weldment dimensional inspection?

A

Weldment dimensional inspection is the measurement of a welded part to confirm its size, hole positions, and geometric tolerances match the drawing. It focuses on the whole part's geometry rather than the quality of individual welds.

Q How do you measure a weldment that is too large for a CMM?

A

Use a portable measuring system that comes to the part instead of moving the part to a machine. A wide-area CMM such as the KEYENCE WM Series tracks a handheld probe with a camera, measuring parts up to 25 m (82 ft) where they sit.

Q Can one person inspect a large, welded frame?

A

Yes. With a wide-area CMM, the camera tracks the probe, so no second person is needed to hold a tape. In one KEYENCE case study, steel members over 10 m that once needed several workers can now be measured by one person.

Q What is the difference between weldment inspection and weld inspection?

A

Weldment dimensional inspection checks the overall geometry of a fabricated part. Weld inspection checks the weld bead itself, such as its position and appearance. Many fabricators need both.

Q Can a wide-area CMM measure hole positions on a weldment?

A

Yes. The contact probe measures single points in space, such as hole centers, without stickers or custom jigs. It also measures distances by touch even when plates or other obstructions sit between the points.

Q Does weldment dimensional inspection support GD&T?

A

Yes. The KEYENCE WM Series contact probe supports 3D and GD&T measurement, and the laser-scanning probe captures shape and form. The system records measurement data and creates inspection reports automatically.

Related Products

Related Downloads