Machine Vision
- Presence/Absence
- Measurement
- Flaw Detection
- Positioning/Alignment
- Character and Barcode Reading
- Line Scan
- 3D Inspection and Measurement
- 3D Vision-Guided Robotic and Bin Picking
- Weld Inspection
- Position Correction
- Advanced Color and Product Type
- Quantity Inspection
- Appearance Inspection
- Dimension Measurement
- Identification & Connector Inspection
- Aerospace
- AI Server and Data Center Component Manufacturing
- Automation Equipment/Machine Building
- Automotive
- Commodities
- Defense
- Electric Vehicles
- Electronic Device
- Fabric/Textile
- Food/Beverage Packaging
- Logistics
- Machine Tools
- Marine
- Medical Device Manufacturing
- Mining/Metals
- Paper Manufacturing
- Pharmaceuticals
- Printing
- Semiconductor/Manufacturing Electronics
- Solar
- Tobacco
- Vision-Guided Robotics
Quantity Inspection Vision System Applications
Modern production lines depend on fast, accurate quantity inspection to keep workflows stable. When count accuracy slips, bottlenecks spread quickly through the line. Product counting systems prevent these issues by verifying part counts in real time and giving operators data they can act on immediately.
A vision system for counting supports this work by capturing high-resolution images and processing them fast enough to match high-speed motion, even when bottling, sorting, or packaging tasks change hour by hour.
Quantity and Counting Applications
Bottle Count in Cases
Using a 21 megapixel camera enables high-accuracy inspection even over a wide field of view. In addition to counting bottles, a single camera enables other inspections, such as the inspection of caps for different types by checking minute differences in characters or colors.
Parts Check Before Oil Filter Assembly
Kitting inspections are possible to ensure the correct parts are included in packages, with accurate counting, even if the position and orientation of the parts vary.
Product Type Differentiation/2D Identification of IC Packages
Read the characters/2D codes laser-marked on the surface of IC chips. A single machine vision system can recognize both characters, such as part numbers, and 2D codes simultaneously.
Chip Count
Count inspections of up to 10,000 chips are possible from a single image rather than the separate images needed by conventional systems.
Cylindrical Battery Count
The IV can reliably count the number of cylindrical batteries, even when there are many. Additionally, since settings can be adjusted instantly, the startup time can be significantly reduced.
Quantity Check for Egg Shipments
Reliable counting of eggs passing on a conveyor is possible regardless of the position or orientation of the eggs.
Candy Bag Quantity Check
The number of candy bags can be counted reliably, even if one is missing from any position or if the shape of the bags is unstable.
Various Part Inspection Inside Tray
Without height data to identify features, it is difficult to inspect an entire tray where there is little contrast on the parts' features and between the parts and the background. If height information from a 3D image is also used, seemingly uniform colors are no longer a barrier to fully inspect the tray. In addition to count, it is also possible to detect different varieties, the difference between front and back, and parts that are oriented incorrectly. LumiTrax™ images* can be obtained at the same time, which eliminates the effects of ambient light and aids in emphasizing the raised features across the tray.
Benefits of Automated Quantity Inspection Systems
Automated quantity inspection gives teams a clear view of how many parts actually move through a station, cycle by cycle. Instead of stopping to count by hand or relying on a quick visual check, the system tracks each item as it enters the field of view and records the result immediately. This approach keeps pace in industries and applications with high-speed lines where small parts, bottles, or mixed components make manual counting unrealistic.
When the system flags a short load or an unexpected increase, operators can look upstream at feed rails, hoppers, or changeover points to find the source before it affects downstream work. The result is steadier throughput and fewer surprises during long shifts.
Key Features of KEYENCE Quantity Inspection Systems
KEYENCE vision platforms strengthen quantity inspection by combining high-resolution cameras and software designed for complex motion environments. With features like multi-spectrum and LumiTrax™ imaging capabilities, the system can capture clear images even when glare, shadows, label curvature, or packaging variations make counting difficult. These features give the system a strong advantage when working with multi-lane operations or mixed materials.
High-speed processors support real-time evaluation during high-volume runs. Even when the line shifts between different shapes or SKUs, programs can switch quickly, helping operators keep throughput constant. Advanced tools in the software also allow the system to track objects across wide fields of view, recognize stacked or overlapping items, and count bottles, packs, or units from a single camera position. For teams managing a bottle counting system, this flexibility reduces setup time and supports steady performance across long shifts.
How Automated Systems Improve Product Counting
Vision-based product counting systems verify quantities by analyzing each frame and tracking individual parts as they move. This makes the process more reliable than fixed sensors that rely on beam breaks or projected spacing. When parts cluster or overlap, the vision system isolates each item using edge detection, pattern recognition, and contrast analysis, producing stable results even when the product mix changes.
Inspection automation also supports downstream accuracy. When a case packer receives reliable count data, reject logic becomes more precise, and fewer cases require rework. The same applies to bottle counting, where fill lines depend on exact quantities to avoid stoppages. Product counting systems help teams maintain flow during long production runs and reduce the number of manual checks needed to keep quality high.
To learn more about how our automated systems can streamline your operations and improve accuracy, explore our automated inspection solutions today.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
FAQs
How Do Quantity Inspection Systems Improve Accuracy in Manufacturing?
They capture each item in real time and apply consistent logic across every cycle. This reduces the variation that comes from manual counting and helps operators maintain steady output during long production runs.
What Industries Use Quantity Inspection Systems?
These systems support food and beverage bottling, consumer goods packaging, electronics assembly, and automotive kitting. Any workflow that depends on reliable part counts benefits from product counting systems.
What is the Key Advantage of Integrating AI Into Quantity Inspection Systems?
AI helps the system adapt when parts overlap, vary in shape, or move unpredictably. It strengthens detection accuracy and keeps counting stable as product types or production conditions shift.
We’re here to provide you with more details.
Reach out today!
Related Products
Related Downloads
Related Information
- Presence/Absence
- Measurement
- Flaw Detection
- Positioning/Alignment
- Character and Barcode Reading
- Line Scan
- 3D Inspection and Measurement
- 3D Vision-Guided Robotic and Bin Picking
- Weld Inspection
- Position Correction
- Advanced Color and Product Type
- Quantity Inspection
- Appearance Inspection
- Dimension Measurement
- Identification & Connector Inspection
- Aerospace
- AI Server and Data Center Component Manufacturing
- Automation Equipment/Machine Building
- Automotive
- Commodities
- Defense
- Electric Vehicles
- Electronic Device
- Fabric/Textile
- Food/Beverage Packaging
- Logistics
- Machine Tools
- Marine
- Medical Device Manufacturing
- Mining/Metals
- Paper Manufacturing
- Pharmaceuticals
- Printing
- Semiconductor/Manufacturing Electronics
- Solar
- Tobacco
- Vision-Guided Robotics