How to Choose the Right Static Control System for Your Industry

Summary: Selecting the right ionizer depends on charge intensity, surface geometry, airflow requirements, and environmental constraints. Static control systems fall into two categories: passive (grounded mats, wrist straps, conductive workstations) and active (ionizing bars, blowers, guns, nozzles). Systems must comply with IEC 61340, ANSI/ESD S20.20, or cleanroom ISO classifications depending on the industry. KEYENCE offers the SJ-F700, SJ-Q, SJ-H, and SJ-E Series for different application profiles. Provided by KEYENCE.

Why does static control matter across industries?

Electrostatic discharge (ESD) affects everything from potato chips to microchips. ESD events can damage sensitive components, attract contaminants, and trigger production errors that compromise output and safety — a single unneutralized charge can delay packaging or skew print alignment.

The consequences of unmanaged static increase as production speeds get faster and material handling becomes more automated. Selecting the right industrial static control system requires a thorough examination of environmental variables, process requirements, and system compatibility.

How do static control needs differ by industry?

In electronics manufacturing, even minor charges can cause latent defects in semiconductors or printed circuit boards (PCBs), leading to intermittent system failures. In pharmaceutical settings, static can attract airborne particles and compromise sterile packaging. In plastics, uncontrolled charges interfere with mold release, precision trimming, and post-processing. Automotive and aerospace facilities manage static both to protect embedded electronics and to prevent paint contamination or overspray.

Each industry's demands are determined by regulatory requirements, cleanliness standards, material flow behavior, and component sensitivity. An ionizer that performs reliably in a cleanroom might be insufficient for a fast-moving extruder line, and conversely, a passive static dissipator suited for packaging may not offer the response time needed for sensitive component assembly.

How do I assess my own requirements?

Before selecting a system, define the operating environment in terms of material characteristics, process speed, and spatial constraints. High-voltage ionizers are suitable for industrial zones with larger clearances, but compact environments require precision-focused systems such as localized nozzles or in-tool ionizers.

Cleanroom environments may need static control equipment certified for ISO class compliance, while ESD prevention strategies demand tools with minimal residual ion imbalance.

It is equally important to determine whether the application involves insulative materials, such as plastics and films, or conductive pathways. Static tends to accumulate in insulative materials that can't dissipate charge naturally.

What types of static control systems exist?

Passive systems use grounded mats, wrist straps, and conductive workstations to allow charge to dissipate naturally. These methods are sufficient for low-risk areas or manual processes where charges build slowly and personnel are directly involved in handling.

Active systems neutralize airborne and surface charges through the targeted release of ions. These include ionizing bars, blowers, guns, and nozzles. Some combine ionization with integrated sensors and automated controls, delivering real-time correction based on charge detection. In environments where production speed and static risk intersect, active ionization is often the only viable solution.

How do ionizers, grounding, and shielding work together?

Ionizers neutralize charge by emitting a balanced stream of positive and negative ions that are attracted to surfaces carrying an opposite charge.

Grounding and bonding are required in systems where charge must be redirected to earth. When used with ionizers, grounding systems provide a complete pathway for charge elimination. Shielding materials may also be used to isolate static-sensitive equipment, preventing environmental charges from interfering with performance.

What features should I look for?

A well-designed system should integrate into the production environment without requiring excessive configuration or upkeep, and must function consistently even in environments prone to high static buildup. Precise charge neutralization matters in sensitive applications where a small residual charge can lead to defects or contamination. Systems that self-monitor or alert operators help reduce downtime.

Easy installation and compatibility with existing infrastructure also matter. Compact footprints, modular components, and flexible mounting options help adapt static control strategies to constrained or evolving production lines.

Maintenance: traditional ionizers require regular cleaning and replacement of probe tips, plus keeping air lines debris-free. KEYENCE's SJ-F700 Series, SJ-Q Series, and SJ-E Series are virtually maintenance-free. The SJ-F700 Series has an auto-probe cleaning function on startup. The SJ-Q Series and SJ-E Series use an "Inside Supersonic Structure" that envelops the electrode probe with coaxial air; this airflow prevents debris build-up on probe tips, allowing probe cleaning reduction to once per year and replacement every 10 years.

Remote monitoring and data collection features support preventive maintenance and system validation. In regulated industries, documentation and traceability features also support compliance with internal audits and external standards.

What factors drive the selection?

For instance, static control in electronics manufacturing may require localized nozzles and minimal airflow to prevent disturbing micro-components. In contrast, plastic packaging lines may benefit from wide-area blowers positioned over conveyor systems.

Which KEYENCE ionizer fits which application?

SeriesTypeBest suited to
SJ-F700 SeriesFan type with powerful airflow, onboard controls, real-time monitoring, automatic balance correctionWide-area applications requiring high-speed neutralization; automotive production, sheet processing, packaging lines
SJ-Q SeriesStatic elimination time of 0.1 seconds, ±3 V ion balance, mountable just 10 mm from the targetCleanrooms, fast-moving lines, electronics handling; removes the need for multiple ionizers along extended transport systems; fits inside tight tooling spaces or enclosed equipment
SJ-H SeriesBar type, air-freeEnvironments requiring airflow-sensitive static control; cleanrooms and applications where zero dust and minimizing particulate movement are essential
SJ-E SeriesLong-range ionization with adaptive power reduction when equipment isn't running, and ion output adjusted by proximity to nearby surfacesProduction lines with intermittent operation or shift-based cycles, where energy savings and reliable static control are both priorities

Frequently asked questions

How do I determine the best static control method for my industry?

Start with an environmental and process risk assessment, then align system features to material type, production speed, and space constraints.

Are there standards or certifications for static control systems?

Yes. Systems must comply with IEC 61340, ANSI/ESD S20.20, or cleanroom ISO classifications, depending on the industry.

What are the common challenges in implementing static control solutions?

Installation in space-constrained areas, maintaining performance over time, and ensuring compatibility with existing equipment.

How do ionizers eliminate static electricity?

They release positive and negative ions that neutralize charged surfaces by restoring electrical balance.

What's the difference between bar, fan, nozzle, and gun-type ionizers?

Bars and blowers handle wide or large areas; nozzles and guns are better for focused or manual applications.

Can ionizer performance be monitored remotely?

Yes. Many advanced systems, including those from KEYENCE, offer real-time sensor feedback and remote monitoring via control interfaces.

Source: KEYENCE, "How to Choose the Right Static Control System for Your Industry" https://www.keyence.com/products/static/resources/static-control-resources/how-to-choose-the-right-static-control-system-for-your-industry.jsp