Industrial Laser Marking Systems / Laser Markers
Laser Marking in the Medical Industry
-
Tags:
- Laser Annealing , Metal , Plastic
Key Takeaways
- Medical device marking supports permanent traceability and identification.
- Medical laser marking creates durable marks on surgical instruments and components.
- Direct part marking helps medical manufacturers meet compliance needs.
- Different materials require different laser marking methods.
- Laser marking systems can integrate into medical production lines.
Medical devices are crucial tools used to diagnose, prevent, or treat various conditions or illnesses. Since these tools are life-altering, they follow a strict regulatory guideline to ensure safety and quality, which requires permanent traceability marks that can be read by humans and machines. Since the majority of medical instruments are small and designed to be used repeatedly after undergoing a disinfection or sterilization process, permanent and legible traceability is difficult. Labels or ink cannot be used in these cases, but laser marking provides the ideal solution for this direct part marking.
What Is Direct Part Marking in the Medical Industry?
Medical laser device marking refers to the process of engraving or permanently marking medical devices with identifying text and/or images. This can include serial numbers, barcodes, logos, and other unique device identifying marks. Laser medical device marking is an alternative to traditional medical device markings, such as printing or stamping.
These device markers offer many benefits over traditional methods, including faster marking speed, the ability to mark small or difficult-to-reach areas, and cleaner and more consistent marks. Additionally, laser marking medical devices provide high resolution marks, utmost accuracy, flexibility, and overall operational efficiency.
Direct marking eliminates consumable costs associated with labels, inks, and adhesives. Production lines run continuously without pausing for label application or ink cartridge replacement. The automated nature of laser marking reduces labor requirements while increasing throughput.
Counterfeit prevention becomes stronger with permanent marks that cannot be removed or altered. The pharmaceutical and medical device industries face ongoing challenges from fraudulent products entering supply chains. Laser-marked serial numbers and 2D codes create authentication systems that protect patients and brand reputation.
Needle hubs
Catheter connectors
Medical tubes
Instrument covers
Small steel objects
Catheter wire
Drill bits
Medical bolts
Medical device laser marking is an essential part of the medical device manufacturing process. This process helps to ensure that each device is accurately and precisely marked. For example, if there is ever a recall of a medical device, the identifying marks can be used to quickly and easily identify which devices are affected. This process is also important for traceability purposes and FDA compliance, as previously mentioned. There are many different types of medical devices that can be marked with lasers, including parts such as stents, dental implants, hip replacements, pacemakers, catheters, and surgical tools, as seen above.
Laser medical marking is a safe, permanent, compliant, and efficient way to mark medical devices. At KEYENCE, we offer high quality laser markers that can meet the needs of any medical application. Our laser medical device markers are backed by our extensive knowledge and experience in the field of lasers and laser applications.
Benefits of Laser Marking for Medical Applications
The medical industry has benefited from laser marking for many reasons. For one, it allows for permanent, high-contrast medical device marking. Important details like serial numbers, barcodes, and logos remain legible through sterilization, wear, and use. For example, laser marking surgical instruments guarantees durable marks on stainless steel and titanium that don't fade, even after repeated autoclaving (the procedure that sterilizes waste, glassware, instruments, and equipment using pressurized steam).
Medical applications do not just require readability. Traceability is also improved with laser marking, reducing the risk of cross-contamination. Properly traced devices allow hospitals and manufacturers to manage their equipment more efficiently. Additionally, the precise nature of laser marking ensures that even delicate medical part marking maintains product integrity, minimizing damage to components.
Quality control is even improved by tracking tool usage. As a result, replacement and ordering schedules are simplified, and efficiency through standardized instrument sets is increased. Better location management and the avoidance of excess stock are made possible by real-time instrument tracking. Analyzing theft and loss is simpler to handle, which improves inventory control.
Reduced Lead Time, Manufacturing Costs, and Environmental Impact
Software Setup
- Reduce manufacturing costs by creating custom programs that adjust for design and part changes.
- Laser marking creates permanent, high-contrast marks without the use of ink.
- Marking can be performed during the manufacturing process, which eliminates the need for extra machinery and additional processing time.
Choosing the Right Laser Marker for the Medical Sector
Choosing the best laser marker for the medical sector depends on the material and the specific needs of the project. Certain lasers excel for laser marking medical devices on metals like surgical tools or implants, while other lasers are ideal for more sensitive materials like plastics used in disposable syringes or medical tubing. Manufacturers typically choose equipment that offers reliable and clear marks on a variety of components. Finding advanced lasers that provide non-contact marking may also be a consideration. Delicate items can be marked without physical stress, preserving their durability and functionality.
When choosing the right laser marker for surgical instruments and medical devices, KEYENCE offers two top systems: the MD-X Hybrid Laser Marker and the MD-U UV Laser Marker. The MD-X blends YVO₄ and fiber lasers for precise, quick marking on metal tools, while the MD-U’s UV technology provides high-contrast, damage-free marks on sensitive materials. Both feature KEYENCE's 3-axis beam control for marking on 3D surfaces and come equipped with advanced Marking Builder software for enhanced automation and ease of use.
Validation techniques guarantee consistent performance across production batches. Equipment qualification methods ensure that marking parameters are stable throughout time. Documentation packages facilitate regulatory audits and quality management system requirements.
Flexibility in programming allows for product line adjustments without substantial retooling. Medical device marking templates that have been stored can be switched between device types in seconds. This versatility allows contract manufacturers to serve various clients with different criteria.
Complex Part Marking
3-Axis Marking
With KEYENCE's Z-MAP Creator software, 3D CAD data (STL format) can be imported directly into the Marking Builder software. The data can then be used as a foundation for three-dimensional marking. Characters and logos can easily be marked on even the most complex shapes with just the touch of a button. Because of its ease of use and high functionality, Z-MAP Creator has become an essential tool in surgical device manufacturing.
Laser Marking Applications by Medical Device Material
Material compatibility determines which laser technology delivers optimal results. Absorption characteristics vary across metals, polymers, and ceramics used in medical manufacturing. Wavelength selection matches the substrate properties to ensure permanent, high-contrast marks without compromising device functionality.
Biocompatibility requirements mandate that medical device marking processes introduce no contaminants or surface alterations that affect patient safety. Non-contact laser systems meet these stringent standards by avoiding physical contact and chemical additives. The process leaves no residue or particles that could trigger adverse reactions.
Laser Marking on Stainless Steel and Titanium Surgical Instruments
Reusable surgical tools demand exceptionally durable marks that withstand repeated sterilization and harsh cleaning protocols.
Direct Marking on Steel Medical Instruments
High-Speed, Precise Marking
Laser markers are used to create identifying marks (like 2D codes) on surgical equipment. These marks are highly visible, don't wear off and can't be erased by chemicals (which is a common problem with pad printers).
Metal Marking on Surgical Instruments
Metal marking on surgical instruments requires marks that survive hundreds of sterilization cycles. Autoclaving exposes devices to high-pressure steam at temperatures exceeding 250°F. Laser-engraved codes withstand these conditions without fading or degrading.
Orthopedic Implants: Orthopedic implants manufactured from titanium alloys accept permanent marks through annealing or ablation techniques. The marks create contrast without removing protective oxide layers that prevent corrosion. Hip replacements, spinal hardware, and dental implants gain traceability while maintaining structural integrity.
Precision Surgical Instruments: Precision scalpels, forceps, and retractors benefit from laser engraving that identifies manufacturer, size, and instrument type. Operating room staff quickly select the correct tools during procedures. Inventory management improves when each instrument carries scannable identification codes.
Laser Marking on Plastic and Synthetic Medical Components
Disposable and single-use medical devices manufactured from polymers require marking methods that preserve material integrity.
Laser Marking Part/Lot Numbers on Medical Tube Connectors
Laser markers can mark both metals and plastics, and they're commonly used to create identifying marks on polycarbonate medical tubing. This identification process is typically accomplished with labels, but they are expensive, take time to produce and run the risk of falling off or being removed. Laser marking eliminates those risks and the costs associated with each.
Direct Marking on Plastic & Synthetic Materials
Permanent, Sharp Markings
Laser marking intravenous bags creates a permanent, easy-to-read mark. Date codes and serial numbers are common marking examples. Ink printing (which is a common marking alternative) easily wears off, and heat stamping is not clearly legible. Replacing either system with a laser solves both issues and eliminates the costs associated with maintenance and consumables.
Plastic marking applications span single-use syringes, drug delivery devices, and diagnostic test cassettes. Polypropylene, polyethylene, and polycarbonate components accept marks without warping or discoloration. UV laser technology prevents heat damage that could compromise sterile barrier integrity.
Blister packaging for pharmaceutical products receives lot codes and expiration dates through laser systems. The marks remain legible throughout distribution and storage without smudging or fading. Regulatory compliance depends on this permanence for patient safety and recall management.
Laser Marking on Catheters, Hypodermic Needles, and Flexible Tubing
Delicate components like catheters and needles present unique medical device laser marking challenges due to their small size and flexible materials. Luckily, the right systems can handle those intricacies.
Laser Processing on the Surface of Catheters
Laser markers can also be used on catheters and hypodermic needles. Cut locations and dwelling positions can be marked in the fluoride coating. Ink systems are commonly used to create these marks, but there's a risk the ink will contaminate the product. Laser markers remove this risk since no chemicals are used in the marking process.
Flexible tubing used in IV lines and drainage systems requires marks that flex without cracking. The laser penetrates just deep enough to create contrast while preserving the tube's mechanical properties. Length markings, French size indicators, and depth graduations guide clinicians during insertion procedures.
Needle gauges and luer connectors carry identification codes despite their miniature dimensions. Beam spot diameters measured in micrometers enable marking on components smaller than a grain of rice. Diabetes patients, nurses, and laboratory technicians rely on these marks for proper device selection.
Ensuring Compliance with Regulations in Medical Device Laser Marking
Compliance with regulations like UDI (Unique Device Identification) is mandatory in the medical field. Medical laser marking is mandated and regulated by the FDA in the United States and the corresponding medical regulatory bodies in other countries. The FDA has established guidelines for unique device identifiers, or UDIs, which must be followed by medical device manufacturers and labelers or markers. These guidelines include specific requirements for various medical device types, such as Class 1, Class 2, or Class 3.
As the FDA site states:
“The FDA established the unique device identification system to adequately identify medical devices sold in the United States from manufacturing through distribution to patient use.
When fully implemented, the label of most devices will include a unique device identifier (UDI) in human- and machine-readable form, which will ultimately improve patient safety, modernize device postmarket surveillance, and facilitate medical device innovation (source).”
These identifiers consist of the device identifier, which is the mandatory mark to identify the device’s version or model. Next is the production identifier, which may include a lot or batch number, serial number, expiration date, and manufacturing date. In order to implement these UDI’s, an accurate laser marking machine that is customized for these specific medical-related requirements must be used.
Medical device laser marking plays a key role in meeting these FDA requirements. Each device must have a scannable, permanent mark for traceability throughout its lifecycle. Laser markers are a common solution, offering the precision needed for this task.
UDIs can be created that are not only readable but can withstand harsh conditions like sterilization or chemical exposure. KEYENCE laser markers are designed to adhere to these strict regulatory standards, offering manufacturers peace of mind in ensuring medical device marking is accurate, durable, and fully compliant. Following the FDA guidelines is essential to ensure patient safety and avoid unnecessary regulatory issues.
Transform Your Medical Equipment with KEYENCE Laser Marking Machines
For manufacturers looking to improve the efficiency and accuracy of laser marking on medical equipment, KEYENCE’s laser markers are an industry-leading choice. Designed to integrate seamlessly into production lines, fast, high-precision marking is easier than ever.
KEYENCE provides a variety of options for various materials and production environments, whether you're marking delicate implants or reusable surgical instruments. Contact us today to start transforming your medical equipment.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
Application Video
FAQs about Laser Marking in the Medical Industry
What’s the Best Laser Engraving Machine for Medical Technology?
UV laser technology was developed with the medical industry in mind. "Cold Marking" capabilities due to improved absorption from the shortened wavelength appeal to many applications in the medical industry due to a decreased HAZ (Heat Affected Zone).
How Are Implants and Surgical Instruments Marked With the Laser Machine?
Implants and Surgical instruments are marked in a variety of ways. The end goal with each marking is implementation of tracking and traceability as well as unique device identification (UDI). 2D data matrix/QR Codes, serialized information, and regulatory logos can all be added via laser marking.
Does Laser Marking Wear Off?
Lasers interact directly with the surface of the material to create a permanent mark. Laser marks will not wear off without fully removing the layers of material that interacted with the laser.
What Are the Different Types of Medical Lasers?
Lasers have nearly endless application potential in the medical industry. Commonly known procedures, such as eye surgery, hair removal, and tattoo removal, utilize laser technology. The laser systems offered by KEYENCE are targeted for production companies in the medical industry to tackle the growing demand for unique device identification (UDI) and selective material processing.
What Are Medical Lasers Used for?
Unique Device Identification (UDI) is a common requirement for medical devices. Lasers are the optimal technology for this as they can provide permanent marks without damaging or compromising the device.
What Is the Minimum Font Size That a Laser Can Mark?
The minimum achievable font size is dependent on the laser's beam spot and is selected based on the material you intend to mark. Under perfect conditions, text sizes as small as 100 µm are possible.
What Is the Best Laser Marking System for Medical Devices?
Material and application requirements will determine the best system for laser marking medical devices. While fiber and hybrid systems are effective for stainless steel surgical equipment and metal implants, UV lasers are excellent for marking heat-sensitive polymers and delicate components.
What Is the Best Laser Engraving System for Medical Devices?
The best laser engraving system depends on the material and application. UV lasers are ideal for heat-sensitive plastics because they minimize heat impact, while fiber and hybrid lasers are commonly used for durable, high-precision marking on surgical instruments and metal implants.
What Types of Medical Devices Can Be Laser Marked?
Surgical instruments, implants, catheters, syringes, IV bags, pacemakers, stents, dental components, and packaging materials can all be marked using laser markers. Permanent laser marks can be applied to both plastic and metal medical components.
Can Laser Marking Systems Integrate With Medical Device Production Lines?
Yes, established industrial standards allow a laser marker for the medical sector to be readily integrated into automated manufacturing lines. For real-time tracking and quality control without interfering with operations, they interact with manufacturing execution systems.
We’re here to provide you with more details.
Reach out today!
Related Products
Related Downloads
-
Practical Solutions of Laser Marking and Part Tracking Traceability Systems
2D codes have become a near-universal standard for traceability. This must-read document covers everything from code scanning principles, laser installation, predictive maintenance, and more.
-
Laser Marker 2D Code Marking for Traceability
2D codes are used to store date codes, lot codes, serial numbers, and more. Users who are considering 2D code marking should read this laser marking guidebook.
-
Laser Marking Equipment Guidebook
Some laser marking applications require integration with multiple devices. KEYENCE provides a total marking solution, from X/Y stages and indexing systems to head traversal systems. Learn more in this brochure.
Scroll