Laser Marking Systems / Laser Markers
- Laser Etching vs Laser Engraving: Which to Choose?
- How Does Laser Cleaning Work?
- What Materials Can Be Marked with a UV Laser Machine?
- EV Laser Marking Applications
- Comparison of Different Types of Electric Vehicle Battery Cells
- Difference Between UV Laser and Fiber Laser Engraving Machines
- How to Choose the Right Laser Marker for Engraving
Laser Marking on Plastic
Laser marking is a reliable and cost-effective technique often used to mark plastic parts. By precisely laser etching plastic surfaces, this equipment produces permanent, high-quality marks. These markings also cause minimal distortion and are resistant to chemicals, abrasion, and extreme temperatures. Common plastics laser-marked include ABS, epoxy, and PET. When laser marking plastic products, the laser light does not penetrate the material. Instead, it chemically or thermally changes its surface according to the laser power intensity within the beam of light.
Laser markings may typically be seen in applications such as brand logos engraved on various appliances and portable electronics, part numbers printed on automotive parts such as brake calipers, or serial numbers etched onto medical tools. As a valuable tool for personalization and customization, laser marking plastic has proven to be a valuable option for manufacturers across numerous industries.
Laser Marking Machine For Plastic
Laser marking machines are an essential piece of equipment for anyone who needs to mark, engrave or print onto plastics. These laser systems use a high-powered laser beam to permanently etch designs or identify code onto plastic components. Depending on the specs and features of each laser marking machine, they can offer outstanding speed, accuracy and reliability while remaining incredibly easy to use.
When selecting the best laser marking machine for plastic materials, it is important to consider its capabilities, how long it takes to set up, how user-friendly it is, and how much maintenance is required. Quality laser markings will last much longer than other processes, such as inkjet printing or mechanical engraving, proving extremely cost-effective in terms of efficiency and longevity.
Major Types of Laser Marking on Plastic
When it comes to laser marking plastic, there are a few main types of processes to achieve the desired results.
Automobile instrument panel switch
Paint peeling
Peel the paint or printing on the target surface to bring out the contrast with the color of the base material.
(Example) Automobile instrument panel switch
Paint peeling has risen in popularity due to its simplicity and convenience. For one, conventional methods (like printing and stamping) require full plate changeovers when a design change occurs. With a laser marker, you can adjust layouts by simply changing the program. For example, in the panel switch example above, if the manufacturer wanted to print on top of the panel switch, it would require custom printing plates. Laser marking makes this task easy as it simply peels the paint off, saving both time and money.
Half cut
Surface layer peeling
Remove/engrave the surface layer with a laser.
(Example) Half cut
Surface layer peeling helps expose the hidden materials beneath our everyday layers, like paint, aluminite, and more. By removing these coatings with this process, a grounding point is created to better access what lies underneath. This enables new possibilities for creativity or problem-solving when it comes to marking on plastic surfaces.
A laser marker can be used to easily process a cutting section. Physical cutters are conventionally used in these scenarios, but they're difficult to adjust and time-consuming to change. Moreover, physical blades must be replaced often (incurring hard costs), and there's a risk that the blade will come loose and get left in the product.
Wide-area marking on LSI
Color development
Irradiate a plastic target with a laser to develop a color in the target itself.
(Example) Wide-area marking on LSI
Color development is used to create beautiful, vivid colors on plastic targets without causing any damage or engraving the material. This common technique allows for personalized customization with creative and unique designs. By using laser radiation to develop a color instead of engraving the plastic, damage from marking the target is minimized.
Welding of transparent plastic and colored plastic
Welding
Use the heat of laser radiation to weld and join plastic parts.
(Example) Welding of transparent plastic and colored plastic
Laser radiation welding offers a reliable and efficient way to join plastic parts, with the added benefit of no vibration, which could negatively affect the product's quality. Without making contact during the process, delicate products remain untouched, eliminating any potential imperfections or damages that may occur due to burrs.
Whatever techniques are chosen, laser marking adds clarity, precision and visibility, making it an ideal choice for long-term results on plastic applications.
Related Downloads

Choosing the right laser marker wavelength is extremely important for plastic marking. Learn what lasers work best for marking, processing, and coloring plastic in this guide.

2D codes have become a near-universal standard for traceability. This must-read document covers everything from code scanning principles, laser installation, predictive maintenance, and more.

2D codes are used to store date codes, lot codes, serial numbers, and more. Users who are considering 2D code marking should read this laser marking guidebook.

Some laser marking applications require integration with multiple devices. KEYENCE provides a total marking solution, from X/Y stages and indexing systems to head traversal systems. Learn more in this brochure.

This booklet covers a wide range of laser processing techniques - such as cutting, drilling, and deep engraving - as well as welding and soldering that are unique to lasers.
Related Products
Application
Industries
Resources
- Laser Etching vs Laser Engraving: Which to Choose?
- How Does Laser Cleaning Work?
- What Materials Can Be Marked with a UV Laser Machine?
- EV Laser Marking Applications
- Comparison of Different Types of Electric Vehicle Battery Cells
- Difference Between UV Laser and Fiber Laser Engraving Machines
- How to Choose the Right Laser Marker for Engraving