Laser Marking Systems / Laser Markers
- Laser Etching vs Laser Engraving: Which to Choose?
- How Does Laser Cleaning Work?
- What Materials Can Be Marked with a UV Laser Machine?
- EV Laser Marking Applications
- Comparison of Different Types of Electric Vehicle Battery Cells
- Difference Between UV Laser and Fiber Laser Engraving Machines
- How to Choose the Right Laser Marker for Engraving
What Materials Can Be Marked with a UV Laser Machine?
There are many types of lasers on the market, such as fiber lasers, CO2, and green lasers. But, a UV laser marking machine is a great choice for an innovative, versatile, and less damaging approach. Unlike fiber or CO2 lasers, UV lasers do not rely on heat pressure to mark materials. Instead, they use absorption levels. Because of the particularly high absorption rate, UV laser marking machines can work on a variety of materials, ranging from plastic to metal.
The high absorption rate is generated from the conversion of a 1064nm laser into a 355nm laser through two crystals. The 355nm then marks by a photolytic degradation process to break the bonds directly.
A UV laser marker breaks the bonds directly instead of ruining the base material like many other laser markers. This process is known as “cold marking” because of the minimal heat stress. Cold marking is effective for high contrast and damage-free marking. In this article, we’ll discuss materials that UV lasers can mark and different UV lasers depending on use.
Because of the high absorption rate of UV lasers, there are plenty of materials that can be marked by a UV laser. UV’s high absorption also allows it to work on mixed materials. Here is a non-exhaustive list of laser-compatible materials that these lasers can handle:
Plastics | Metals | Other materials |
---|---|---|
Plastics
|
Metals
|
Other materials
|
Here’s a non-exhaustive list of products that a UV laser could mark in different industries:
Automotive | Electronics | Medical | Food/Cosmetics/etc |
---|---|---|---|
Automotive
|
Electronics
|
Medical
|
Food/Cosmetics/etc
|
The Best UV Laser Marking Machine for Any Material
3 Axis UV Laser Marker
For materials like metals, plastics, and glass, the 3-Axis UV Laser Marker MD-U Series is a great option for versatility. The MD-U Series generates detailed, damage-free, and high-contrast marking on a range of shapes, materials, and sizes. Additionally, the MD-U Series creates neat plastic cuts without heat effects, burrs, and yellow tinting.
Unlike a conventional laser cylindrical target, the MD-U Series has a 3-Axis control that creates distortion-free marking. The 3-Axis control uses a uniform line width across a marking area of 300mm x 300mm. Because of this, all characters will have the same shape and thickness from edge to edge. Additionally, the 3-Axis system has software that de-focuses each target to eliminate mismarking and distortion.
The MD-U 3-Axis also understands a variety of targets, including 3D stepped, inclines, cylindrical, and cone targets. Even if a target does not fit into those shape categories perfectly, you can upload the profile of the target into MD-U’s Marking Builder 3. The MD-U will understand the profile and mark it appropriately without distortion. This is beneficial for objects like tablets, tubes, earbuds, and other odd-shaped parts.
The MD-U can create many markings such as:
- Logo filling
- 2D code pattern creation
- Fonts
- Barcodes
- GS1 Databar
Final Thoughts
No matter what industry you are in, a UV laser marking machine can improve work time, decrease product damage, and produce higher quality marks or cuts. Using a UV laser significantly cuts down costs because of its ability to work on a wide range of materials, shapes, and products.
KEYENCE is a leading supplier of laser marker technologies worldwide with a 3-Axis System, built-in viewfinders, and the ability to mark products of various shapes and sizes.
Ready to incorporate UV lasers into your projects? If you still have questions, Ask KEYENCE, and our knowledgeable team will get back to you quickly. We support our customers from the selection process to operations with on-site operating instructions, along with industry-leading after-sales support.
Related Products
Application
Industries
Resources
- Laser Etching vs Laser Engraving: Which to Choose?
- How Does Laser Cleaning Work?
- What Materials Can Be Marked with a UV Laser Machine?
- EV Laser Marking Applications
- Comparison of Different Types of Electric Vehicle Battery Cells
- Difference Between UV Laser and Fiber Laser Engraving Machines
- How to Choose the Right Laser Marker for Engraving