Continuous Inkjet Printers / Case Coder
Materials and Products
Production Machines
Printing Applications
Non-Contact Inline Printing on Paper Bag Packaging
Key Takeaways
- KEYENCE's multi-sensing unit detects speed, height, and vibration in real time to prevent distorted codes on paper bags.
- Use fast-drying, high-contrast inks designed for porous kraft paper to maintain barcode and text legibility.
- Continuous inkjet printers offer long throw distances, ensuring sharp codes on uneven or bulging filled bags.
- Integrating smart sensing printers reduces manual adjustments and downtime across variable packaging lines.
Paper bags move through filling, sealing, and case packaging lines at a pace that leaves little room for marking errors. Information like lot codes and expiration dates has to be applied to a variety of substrates that can shift in height and position as they move through production. For manufacturers that rely on paper bag packaging printer systems, industrial continuous printing offers a practical way to add variable data without needing to interrupt throughput.
Unlike decorative package printing performed off-line, coding on paper bags happens inside an active production environment. The printer must work alongside conveyors, respond to speed changes, and apply legible marks on porous kraft surfaces.
Challenges of Printing on Paper Bags
Paper bag substrates introduce variables that do not typically occur when handling rigid cartons. Most paper bags are made with a brown kraft material that absorbs ink quickly. This can soften the edges of a barcode or expiration date if the ink formulation is not formulated for the surface on which it is being printed. Fiber texture and natural color also influence how data appears once dried.
Post-fill coding can add another layer of complexity. Once a bag is filled, the surface may bulge or wrinkle. Gussets and seams can also create uneven print zones. If the distance between the printhead and substrate is too great, then the sharpness of the code (or other information) suffers.
Production environments can also influence the challenges of package printing. Flour, feed, powders, or granular materials can release dust that can settle near the print zone. Vibrations from the production line and conveyors affect alignments, and temperature shifts can alter behavior.
Stretched or compressed codes
Wavy codes
Adjusting Printhead for Variable Bag Speed
Speed variations caused by conveyor changes, gaps, or misfeeds make it difficult to maintain consistent code alignment. Systems that rely on static triggers or encoder timing can’t adapt mid-run, often producing stretched or compressed codes.
Manual adjustments become routine when coding on bagging lines. Each new product or speed setting can introduce fresh inconsistencies, especially if bag dimensions or spacing fluctuate between runs. These setup delays add cost and complexity for teams managing packaging machine coding across variable products.
MSU Speed Compensation for Bags
Zero print distortion
KEYENCE multi-sensing unit (MSU) enables precise print control by actively detecting speed, height, and bag movement during operation. The MSU adjusts print timing in real time, compensating for product variation and delivering distortion-free codes across all bag types.
MSU-equipped systems provide dependable inkjet coding for paper bags, reducing error rates without slowing throughput. No additional encoders or line modifications are required.
Vibration Detection on Form-Fill Lines
Different types of conveyors, including roller conveyors, can cause vibrations, vertical movement, and misalignment, where the leading and trailing edges of the package may not be level, all of which disrupt print positioning.
The MSU eliminates these issues by detecting vertical movement or flutter before printing begins, preventing nozzle collisions, print misalignment, and the need for repeat runs.
Ink Selection for Porous Paper
Uncoated paper bags pull in ink differently than film or foil packaging. Without the proper ink formula, the ink can bleed into the fibers, causing barcodes to lose definition. To avoid this, many production teams use high-contrast inks developed specifically for porous substrates. Continuous inkjet and high-resolution printers support these ink types, maintaining code legibility even at higher speeds.
Integration with Bag Handling Systems
Paper bag packaging machines
Flat pouch conveyors and form-fill-seal machines don’t always deliver consistent bag height or orientation. For bagging lines that change formats or materials frequently, this kind of flexibility is essential to maintain print consistency without constant adjustment.
Systems built for integration, like inkjet printers for packaging machines with smart sensing and compact footprint, simplify setup and reduce the need for custom mounts or manual adjustment. Fewer changeovers, fewer failures, and more uptime.
Visit our product page to explore how the CC-1000 Series delivers reliable paper bag printing across demanding applications.
Industrial Printers for Paper Packaging
Continuous inkjet (CIJ) printing is widely used for coding on flexible and semi-rigid packaging. In industrial inkjet printing, ink droplets are generated continuously and directed toward the substrate in question. Because the printhead does not touch the bag, clear information can be printed on curved or shifting surfaces.
KEYENCE produces the MK-G Series, which supports high-speed variable data printing for primary packaging. Lot codes and expiration dates can be updated automatically. The MK-G Series also supports quick-drying pigment inks that adhere to paper surfaces, which also minimize any ink transfer to guides or belts.
Package Printing for Production Machines
Paper bag lines often combine form-fill-seal equipment with downstream conveyors and other equipment. A paper bag printer must integrate into these stages without adding manual intervention.
Flat-form bag coding differs from post-fill coding. When bags are printed before filling, most surfaces remain uniform and easier to position. After filling, guide rails may be needed to help stabilize the bag as it moves through the print zone. Packaging printers that tolerate slight misalignment provide greater flexibility across different product formats.
High-Speed Coding on Paper Bag Lines
High-volume operations demand consistent performance regardless of speed. If characters stretch or compress throughout the production process, it affects how readable the barcode is. Encoder-driven Case coding compensates for speed variation, so character height and width remain stable.
Throw distance becomes important when bags are not perfectly flat. The CC-1000 Series is designed with a long-distance capability that helps reduce the risk of head contact while preserving how sharp a marking appears. This is especially useful on woven or heavy-duty paper that is used in industrial packaging.
Choosing a Packaging Printer for Paper Bags
Selecting a packaging printer for paper bag application starts with understanding the required font size. Thin retail bags differ from multi-layered industrial sacks. Some jobs require more compact lot codes, while others demand a larger and more scannable barcode for distribution. Substrate absorbency and surface consistency directly affect how inks spread and how sharply characters are printed. Line speed and product spacing also determine how tightly the print has to move product throughout the line.
Primary bag coding generally calls for a system that can maintain proportional text as conveyors increase and decrease speed. Matching a printer's capabilities to each stage of the packaging process helps reduce any integration challenges and limits how production can be disrupted.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
FAQs
Can Inkjet Codes Dry Fast Enough on Porous Bags?
Yes, fast-drying inks specifically designed for paper help to minimize smearing.
Does MSU Detect Bag Flutter Before Printing?
Yes, it automatically detects vibration and vertical motion, ensuring accurate print alignment.
What Traceability Standards Apply to Food-Grade Bags?
Commonly, GS1-compliant barcodes and date coding are required.
Can the MSU Work With Different Types of Conveyors?
Yes, it adjusts for height, speed, and motion in real time across various conveyor types.
How Can Inkjet Coding on Paper Bags Reduce Production Downtime?
Automated adjustments, diagnostics, and simple maintenance reduce errors and recovery time.
We’re here to provide you with more details.
Reach out today!
Related Products
Related Downloads
Related Information
Materials and Products
- Glass Bottles
- Plastic Bottles/Containers
- Cans
- Wires, Cables, & Pipes
- Pouches
- Metal Parts
- Corrugate Boxes
- Packaging Film
- Kraft Packaging
- Folding Cartons
- Building Materials
- PCBs
- Cartons
- Pallets & Lumber
- Corrugate Trays
Production Machines
- Paper Bag Packaging
- Box Conveyor
- Automatic Palletizer
- Sealer/Taping Machine
- Bottle Filling Machine
- Flow Wrapper
Printing Applications