Continuous Inkjet Printers / Case Coder
Materials and Products
Production Machines
Printing Applications
Case Coding for Sealers and Taping Machines
For many operations, the last step before shipment—printing accurate, readable codes on sealed cartons—is critical for compliance and traceability. Integrated with automated taping machine case coding systems or sealing machines, the right case coding solution ensures each package leaves the line with durable, scannable information applied at full speed.
Where Case Coding Meets Case Sealing
Case sealing locks in product protection, but pairing it with case sealer printing adds traceability and compliance without slowing the line. Applying codes during sealing helps prevent adhesion issues with labels, especially on tape seams or textured corrugated materials.
When done correctly, taping machine case coding delivers traceable shipments that can be tracked through every stage of the supply chain. It ensures regulatory compliance for industries where product and batch details must be visible, producing durable, high-resolution prints that withstand handling and storage. Finally, it enables faster throughput by combining sealing and automated case marking in a single step.
For mixed product runs, an inline case coder like the CC-1000 Series applies this data consistently, without operator input.
We’re here to provide you with more details.
Reach out today!
Key Integration Points with Taping Machines
An inline case coder must match the pace and movement of the sealing line, not just bolt onto it. Look for systems that can:
- Mount in a position that keeps the coder close to the case without blocking the sealer’s operation.
- Match the sealer’s throughput, adjusting on the fly as conveyor speed changes.
- Compensate for vibration or minor case height differences to keep codes sharp.
- Exchange start/stop and status signals with upstream and downstream equipment, such as case erectors or palletizers.
The CC-1000 Series addresses each of these points with adaptable mounting, a Multi-Sensing Unit for real-time adjustments, and a single control panel for both printing and inspection.
Real-Time Sync with High-Speed Lines
Fully automatic sealers can run up to 30 cases per minute. At these speeds, traditional coders can experience issues with stretched barcodes or misplaced prints. The CC-1000 Series’ Multi-Sensing Unit tracks speed, detects vibration, and adjusts print timing. This means case sealer printing remains sharp and scannable, even on freshly taped surfaces.
Curious about our pricing?
Click here to find out more.
Choosing the Right Inkjet System
Sealing lines need coders that handle varied corrugate finishes, tape seams, and vibration. A large character inkjet printer with a long throw distance avoids smears, prevents splashback, and maintains code clarity without touching the case. The CC-1000 Series delivers on these features while also printing at 360 DPI resolution for sharp barcodes and graphics, even on mixed case and box sizes.
CC-1000 Series Advantages in Sealing Environments
- Integrated inspection for barcode grading and presence verification
- One-touch head replacement to cut downtime
- Cleaning module to prevent nozzle damage and clogs
- Centralized control for both print and inspection functions
These features keep automated case marking reliable at high speeds and across multiple case formats.
Common Mistakes to Avoid in Print Positioning
On a sealing line, several factors can throw coding off target, such as positioning the printhead too close to the case, which increases the risk of splashback or nozzle clogging, or ignoring the vibration from roller conveyors, which disrupts stability. Running a system without effective speed tracking can further distort barcode dimensions when even minor conveyor speed changes occur. With features like vibration detection, real-time speed compensation, and a long throw distance, the CC-1000 Series maintains consistent placement even when conditions vary from one case to the next.
Make Every Sealed Case Print-Perfect
Contact us today to learn how the CC-1000 Series can integrate with your sealing line for high-speed, high-quality taping machine case coding.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
FAQs
Can a Taping Machine Coder Print on Both Sides of a Case?
Yes, with the right configuration, a taping machine coder can print on multiple sides of a case in a single pass, ensuring efficient and accurate coding with minimal downtime.
How Do I Avoid Smearing When Coding on Fresh Seals?
To avoid smearing when coding on fresh seals, maintain the proper throw distance and use a non-contact system that adjusts for line speed to ensure clear, reliable marks.
What Maintenance Is Required for Taping-Integrated Coders?
Minimal maintenance is required. Systems like the CC-1000 Series feature automated cleaning and on-site quick-change printheads, which reduce downtime and ensure continuous, high-performance operation.
We’re here to provide you with more details.
Reach out today!
Related Products
Related Downloads
Related Information
Materials and Products
- Glass Bottles
- Plastic Bottles/Containers
- Cans
- Wires, Cables, & Pipes
- Pouches
- Metal Parts
- Corrugate Boxes
- Packaging Film
- Kraft Packaging
- Folding Cartons
- Building Materials
- PCBs
- Cartons
- Pallets & Lumber
- Corrugate Trays
Production Machines
- Paper Bag Packaging
- Box Conveyor
- Automatic Palletizer
- Sealer/Taping Machine
- Bottle Filling Machine
- Flow Wrapper
Printing Applications