Continuous Inkjet Printers / Case Coder
Materials and Products
Production Machines
Printing Applications
Direct Printing vs. Labeling on Cardboard: Which Is Better
Key Takeaways
- Direct printing doubles line throughput vs. label applicators and removes label handling steps.
- Switching to inkjet reduces consumable costs; studies show 50–60% savings per 1,000 prints.
- Modern inkjet (360 dpi, inspection cameras) achieves reliable, scannable barcodes on corrugated.
- Limitations: substrate contrast, placement, and some ANSI-compliance needs may still require labels.
Every product shipped through a distribution network relies on cardboard boxes to carry not only goods, but the data that keeps supply chains moving. These cartons often display barcodes, lot numbers, expiration dates, and shipping information that must remain readable from the packaging line through warehouses and final delivery.
Traditionally, many manufacturers have relied on labeling systems to apply this information to cartons. However, as production volumes increase and operations look for ways to reduce cost and complexity, direct printing on cardboard has become a widely used alternative. Both methods offer advantages, and the best choice depends on how speed, cost, print quality, and operational requirements align with a facility’s packaging workflow.
Why Direct Printing on Cardboard Saves Time and Money
One of the strongest advantages of direct printing on cardboard is speed. Labeling requires multiple steps—printing the label, dispensing it, and applying it to the carton—which adds handling points to the packaging line. By contrast, an inkjet printhead applies information directly to the carton as it moves past on a conveyor, eliminating label handling altogether.
In many carton‑coding applications, large‑character inkjet printing can run at nearly twice the throughput of label applicators. Direct printing also reduces ongoing consumable costs. Labels require substrates, adhesives, ribbons, and storage space, while direct printing primarily relies on ink. Studies of carton operations often show significant cost reductions per 1,000 prints when switching from labeling to direct printing, especially in high‑volume environments.
How Barcode Readability Differs Between Direct Printing and Labels on Cardboard
Barcode readability plays a critical role as cartons move through conveyors, warehouses, and distribution centers. Labels provide a uniform, high‑contrast surface that supports consistent barcode scanning regardless of carton material. For this reason, many logistics networks standardize label formats for outbound shipments.
Direct printing on cardboard relies on ink absorption into a porous surface. Modern inkjet systems are designed to produce scannable barcodes on corrugated cartons, but print quality can vary based on carton color, fiber texture, and ink formulation. Lighter cartons generally offer higher contrast, while darker or recycled cardboard may require print optimization to maintain scan reliability.
In operations where cartons must pass through multiple scanning points, validating barcode performance under real production conditions helps determine whether direct printing meets requirements or whether labeling remains necessary.
The Durability Advantage of Direct Inkjet Printing on Cardboard
Durability matters as cartons travel through warehouses and distribution centers where exposure to dust, handling, and abrasion can affect printed information. Labels provide excellent print clarity and contrast, particularly when paired with thermal‑transfer printing on white label material.
Direct printing on cardboard has advanced significantly. Modern inkjet systems with higher resolution and inspection capabilities can produce readable markings on corrugated surfaces. However, factors such as carton absorbency and surface texture still influence final print appearance, making application testing an important part of equipment selection.
Compliance and Retailer Requirements for Carton Identification
Some distribution networks and retailers enforce strict requirements for carton identification, including barcode placement, contrast ratios, and standardized logistics label formats. In these environments, labeling systems remain the preferred solution regardless of production speed or material cost.
Direct printing is commonly used upstream in manufacturing, internal logistics, and pallet‑level identification, while labeling is often reserved for shipments entering retail or third‑party distribution systems with predefined compliance standards. Understanding where cartons will travel—and which systems will scan them—helps determine whether direct printing on cardboard is suitable for the entire packaging workflow or best used alongside labeling systems.
Using Direct Printing and Labeling Together on the Same Packaging Line
Many packaging operations do not rely exclusively on one method. Instead, they combine direct printing and labeling within the same workflow.
In these hybrid setups, direct printing applies core traceability data—such as production dates, lot codes, or internal tracking information—directly onto the carton during packing. Labels may then be applied later to meet shipping, customer, or retailer‑specific requirements.
This approach allows manufacturers to reduce label usage while maintaining compliance where required and supports flexible packaging strategies across multiple distribution channels.
When Direct Printing on Cardboard Makes Sense
Direct printing is well‑suited for high‑volume operations focused on streamlining packaging workflows. Facilities that ship large quantities of corrugated cartons often favor solutions that integrate directly into automated packaging lines. Direct printing reduces material handling, simplifies consumable management, and supports rapid throughput on production lines.
Situations Where Labeling May Be the Better Option
While direct printing on cardboard offers advantages in speed and material reduction, it is not ideal for every application. Labeling may be better suited when cartons vary significantly in color or surface quality, when extremely high barcode contrast is required, or when large amounts of detailed information must appear on the package.
Labeling systems also provide greater flexibility for angled application, corner wrapping, or placement changes on cartons of varying sizes. In packaging environments with strict logistics or retailer requirements, these factors often make labeling the preferred solution.
Choosing the Right Method for Your Operation
Both direct printing and labeling play important roles in secondary packaging. The best solution depends on production speed, scanning requirements, compliance needs, and how cartons move through the supply chain. Evaluating these factors helps determine whether direct printing on cardboard, labeling, or a combination of both delivers the best long‑term performance for your operation.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
FAQs
How Does Direct Printing on Cardboard Compare to Labeling in Terms of Cost-Efficiency?
Direct printing eliminates label material, ribbons, and related storage, cutting costs by as much as 50 to 60 percent. Printing carton labels requires ongoing consumables, while direct coding uses only ink.
What Types of Ink Are Best Suited for Printing Directly on Cardboard?
Specialized inks formulated for porous surfaces provide the strongest results. These inks dry quickly and maintain contrast on corrugated stock.
Can Direct Printing on Cardboard Withstand the Wear and Tear of Shipping and Handling?
Yes. With high-resolution heads, long throw distances, and inspection systems, modern direct printing delivers codes that remain legible throughout logistics.
We’re here to provide you with more details.
Reach out today!
Related Products
Related Downloads
Related Information
Materials and Products
- Glass Bottles
- Plastic Bottles/Containers
- Cans
- Wires, Cables, & Pipes
- Pouches
- Metal Parts
- Corrugate Boxes
- Packaging Film
- Kraft Packaging
- Folding Cartons
- Building Materials
- PCBs
- Cartons
- Pallets & Lumber
- Corrugate Trays
Production Machines
- Paper Bag Packaging
- Box Conveyor
- Automatic Palletizer
- Sealer/Taping Machine
- Bottle Filling Machine
- Flow Wrapper
Printing Applications