Static Control
- Multi-Sensor Ionizer SJ-F700 series
- High-Accuracy High-Speed Sensing Ionizer SJ-Q series
- Energy-Saving High-Speed Sensing Ionizer SJ-E series
- Air-Free High Speed Sensing Ionizer SJ-H series
- Compact Nozzle Static Eliminator SJ-LM series
- Ultra-durable, High-power Static Elimination Gun SJ-LG series
- Compact Fan Static Eliminator SJ-LF series
- High-Performance Micro Static Eliminators SJ-M series
- High-Accuracy Inline Electrostatic Sensor SK series
- Electrostatic Sensor SK-H series
Static Control Solutions to Prevent Staff Discomfort
Static shocks are easy to dismiss, but static electricity discomfort in workplaces creates more than momentary irritation. Staff dealing with repeated jolts lose focus, and over time, the irritation becomes a source of distraction. The same discharges also interfere with equipment, shortening component life or disrupting performance. What seems like a minor spark can shorten the life of electronic boards, scramble sensors, or, in sensitive settings, create fire hazards.
We’re here to provide you with more details.
Reach out today!
The Hidden Impact of Static on Employee Workplace Safety
Static shocks are easy to dismiss until their impact becomes clear. Studies in electronics and office environments have linked as much as 80% of computer and electronic failures to static electricity. In high-precision sectors, even small discharges lead to latent device damage that may not show immediately, but shortens the lifespan of components. For employees, this translates into repeated static electricity discomfort in workplaces and lost productivity when shocks occur throughout the day.
Why Staff Experience Shocks in Controlled Environments
Even in facilities designed with strict controls, static often finds a way. Dry air or low humidity is one of the main culprits, as once humidity dips below about 40%, charges build quickly, and the problem worsens during the winter season. Floors covered in carpet, synthetic uniforms, and constant airflow from HVAC systems or production equipment add more friction to the mix. That combination makes preventing shocks from static electricity a routine challenge in both office and industrial settings.
Cleanrooms and laboratories face their own version of the problem. Staff moving across conductive flooring still generate a charge that can discharge into delicate instruments or into their own bodies.
Creating a Safer, Shock-Free Workplace
Traditional methods of reducing shocks focus on local solutions; mats, footwear, and grounding straps reduce shocks at specific points, but they leave wide areas unprotected. Anti-static sprays and clothing can also help. Adding ionizers elevates this to true ESD safety for staff across work areas.
More advanced facilities layer these approaches with engineering controls. Humidity control keeps the air from drying out, and conductive flooring drains charge through footwear into the ground.
However, the strongest results for staff comfort come from addressing static before it reaches people or equipment. Ionizers make this possible by releasing positive and negative ions that neutralize surface charge on tools, materials, and workers; all of this helps eliminate static shocks and maintain an anti-static workplace.
Discover more about this product.
Click here to book your demo.
KEYENCE Anti-Static Solutions for Personnel Comfort
Ionizers can be applied across an entire production floor, giving broader coverage than local fixes like mats or sprays. KEYENCE systems are built to match different workplace needs.
The SJ-Q Series is suited for tight spaces where mounting flexibility matters, while the SJ-E Series brings high-speed charge removal to fast-moving lines. For wider areas, such as conveyors or large assembly stations, the SJ-H Series provides bar-type coverage. Together, these options allow facilities to select the configuration that best fits their layout.
These systems deliver stable ion balance without the need for frequent adjustments or consumables, making them more practical than mats or sprays. By addressing the air around employees and work surfaces, KEYENCE ionizers remove the charge that causes both ESD safety concerns for staff and electronic failures.
Industries Where Static Affects Human Safety
Static shocks affect nearly every industry. In electronics and semiconductor work, they damage sensitive parts, whereas in pharmaceutical and food plants, they disrupt cleanrooms and complicate powder handling. Even offices and labs report frequent complaints tied to dry air and carpeted floors.
Because the problem cuts across industries, safety and comfort go hand in hand. Eliminating static protects staff, keeps production steady, and reduces downtime. Addressing this hidden hazard creates conditions where people and technology perform reliably.
Create a static-free workspace today by exploring KEYENCE ionizer solutions and bringing greater comfort and safety to your team. Contact us to learn more today!
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
FAQs
How Can I Test Static Levels in Employee Zones?
Facilities typically monitor static using handheld meters or through routine inspections tied to safety programs.
Are Anti-Static Floor Mats Enough for Staff Comfort?
Mats help at individual workstations but do not eliminate static across an entire facility. Ionizers provide broader coverage.
What Industries Face the Most Static-Related Staff Complaints?
Electronics, cleanrooms, automotive, pharmaceutical, and office environments report the highest incidence of static electricity discomfort in workplaces.
We’re here to provide you with more details.
Reach out today!